Additional Uplink parameters are described in Cell Parameters (Basic LTE FDD Uplink), PUCCH Common (Basic LTE FDD Uplink), and Sounding Reference (Basic LTE FDD Uplink).
|
2. PUSCH Common |
|---|
Click this cell and then the
button to open the Configure PUSCH Auto-calculate
window where you can set PUSCH Common parameters.
Displays the state for automatic calculation of per-slot parameters. To change the displayed state, refer to Set PUSCH Auto-calculate per slot params above.
Displays the value for PUSCH nDMRS(1). This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211). To change the displayed value, refer to Set PUSCH Auto-calculate per slot params above.
Displays the value for PUSCH nDMRS(2). This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211). To change the displayed value, refer to Set PUSCH Auto-calculate per slot params above.
Displays the value for PUSCH Delta SS. This value is used to calculate the sequence-shift pattern (see 3GPP TS36.211). To change the displayed value, refer to Set PUSCH Auto-calculate per slot params above.
Displays the state for PUSCH Frequency Hopping. To change the displayed state, refer to Set PUSCH Auto-calculate per slot params above.
Displays the PUSCH frequency hopping mode (see 3GPP TS36.211).
Displays the PUSCH frequency hopping type (see 3GPP TS36.211).
Displays the PUSCH Frequency Hopping Offset value (see 3GPP TS36.211).
Displays the number of sub-bands (Nsb) (see 3GPP TS36.211).
Displays the value for CURRENT_TX_NB mod 2 (see 3GPP TS36.211).